cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX DSP BUG

ALO9611
Associate II

在使用CubeMX生成Makefile工程文件时,在Mid中间件选项中选择“X-CUBE_ALGOBUILD”选项,并添加DSP Library,但是在最后的生成的项目文件中并没哟dsp.lib文件,应该是一个bug,望修复

6 REPLIES 6
TDK
Guru

> When using CubeMX to generate the Makefile project file, select the "X-CUBE_ALGOBUILD" option in the Mid middleware option and add the DSP Library. However, there is no dsp.lib file in the final generated project file. This should be a bug. hope to repair

If you feel a post has answered your question, please click "Accept as Solution".

Yes,this is what i mean

Hello,

First let me thank you for posting.

Can you provide please the STM32CubeMx version.

Thanks.

Mahmoud.

6.9.1

Hello @ALO9611 @TDK ,

For more investigation, I suggest that you provide the ioc.file.

Thanks.

Mahmoud.

应该是我的中文路径影响到了,同时我也没找到那天我创建的文件夹,今天我又试了试,可以了