2024-01-26 3:22 AM
在使用CubeMX生成Makefile工程文件时,在Mid中间件选项中选择“X-CUBE_ALGOBUILD”选项,并添加DSP Library,但是在最后的生成的项目文件中并没哟dsp.lib文件,应该是一个bug,望修复
2024-01-26 6:23 AM
> When using CubeMX to generate the Makefile project file, select the "X-CUBE_ALGOBUILD" option in the Mid middleware option and add the DSP Library. However, there is no dsp.lib file in the final generated project file. This should be a bug. hope to repair
2024-01-26 6:33 AM
Yes,this is what i mean
2024-01-29 1:10 AM
Hello,
First let me thank you for posting.
Can you provide please the STM32CubeMx version.
Thanks.
Mahmoud.
2024-01-29 2:14 AM
6.9.1
2024-01-30 12:14 AM
2024-01-30 2:33 AM
应该是我的中文路径影响到了,同时我也没找到那天我创建的文件夹,今天我又试了试,可以了