cancel
Showing results for 
Search instead for 
Did you mean: 

about STM32CubeMx

JChen.37
Associate II

This morning, I installed cubemx and created a project for STM32F767IGT6 

using J-link v2 to download the hex file to the board, but it didn't work.

The project have included the LTDC, but I cannot get any signal(DCLK/VSYNC/HSYNC)

from the test pads on PCB. It looks like the system clock(216MHz) doesn't work or

something wrong. The board is good and works fine with my the other project hex files.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JChen.37
Associate II

I install CubeMX IDE and try the same settings again.

Now the HID-USB and LTDC does work now.

I will check the settings of CubeMx again.

View solution in original post

5 REPLIES 5
Aymen ABBES
ST Employee

Hello, 

First of all let me thank you for posting.

Could you please provide the *.ioc file and the CubeMx and CubeIDE version so I be able to investigate the issue.

Kind regards,

Aymen

JChen.37
Associate II

Hi Aymen,

Thanks for your support.

Attachment is the ioc file and the CubeMx version is 6.6.1

IDE software is MDK-ARM 5.2.1.

I also attach the download link of complete cubemx project.

JChen.37
Associate II

Here is ioc file.

There's always the debugger..

​

P​erhaps instrument Error Handler and Hard Fault Handler, see if it dies there.

​

C​heck HSE_VALUE, and that clock starts and PLLs lock.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
JChen.37
Associate II

I install CubeMX IDE and try the same settings again.

Now the HID-USB and LTDC does work now.

I will check the settings of CubeMx again.