cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMonitorPWR Software not working for linux

LR.2
Associate III

Hey Guys,

I downloaded STM32CubeMonitorPWR software for linux from officail site - link.

After Downloading when i try to unzip the file it shows "There was an error while extracting the file." Can anyone help me with this.

LR2_0-1687864426986.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Well, 60.3MB is a rounded number, which is why I asked for the file size in bytes, which by the way is 60'292'403 in version 1.2.1. But at least the checksum is already incorrect, correct would be: 9F8E3CAD09F734B13151F3DA5828465879AAB4F8F7E26BA4A1DA17E0A97109E6

Please repeat the donwload again.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

The ZIP archive was probably damaged during the download.

  • What is the file size (bytes) of the ZIP?
  • Can you determine the checksum SHA-256?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

The file size is 60.3 MB and the checksum SHA-256 is 

5e9196eff0da4693a4ec7759c1ae22c740f033aa9c3ab2a424f7b8dff07989b7

File Name: en.CubeMonPwr-Lin.zip

Regards,

Lakshmanan

Peter BENSCH
ST Employee

Well, 60.3MB is a rounded number, which is why I asked for the file size in bytes, which by the way is 60'292'403 in version 1.2.1. But at least the checksum is already incorrect, correct would be: 9F8E3CAD09F734B13151F3DA5828465879AAB4F8F7E26BA4A1DA17E0A97109E6

Please repeat the donwload again.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

Thanks I downloaded again and it worked fine. Also, I checked the checksum its the same as you mentioned. Earlier I tried downloading in different PC's but still the issues existed know I can able to download and extract properly.

Regards,

Lakshmanan

Peter BENSCH
ST Employee

Great!

If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.