2023-07-05 12:36 AM - last edited on 2023-07-05 1:53 AM by Carmelo VICCICA
Hey Guys,
I downloaded STM32CubeMonitorPWR software for linux from officail site - link.
After Downloading when i try to unzip the file it shows "There was an error while extracting the file." Can anyone help me with this.
Solved! Go to Solution.
2023-07-05 3:22 AM
Well, 60.3MB is a rounded number, which is why I asked for the file size in bytes, which by the way is 60'292'403 in version 1.2.1. But at least the checksum is already incorrect, correct would be: 9F8E3CAD09F734B13151F3DA5828465879AAB4F8F7E26BA4A1DA17E0A97109E6
Please repeat the donwload again.
Regards
/Peter
2023-07-05 3:02 AM
The ZIP archive was probably damaged during the download.
Regards
/Peter
2023-07-05 3:08 AM
Hi Peter,
The file size is 60.3 MB and the checksum SHA-256 is
5e9196eff0da4693a4ec7759c1ae22c740f033aa9c3ab2a424f7b8dff07989b7
File Name: en.CubeMonPwr-Lin.zip
Regards,
Lakshmanan
2023-07-05 3:22 AM
Well, 60.3MB is a rounded number, which is why I asked for the file size in bytes, which by the way is 60'292'403 in version 1.2.1. But at least the checksum is already incorrect, correct would be: 9F8E3CAD09F734B13151F3DA5828465879AAB4F8F7E26BA4A1DA17E0A97109E6
Please repeat the donwload again.
Regards
/Peter
2023-07-05 4:27 AM
Hi Peter,
Thanks I downloaded again and it worked fine. Also, I checked the checksum its the same as you mentioned. Earlier I tried downloading in different PC's but still the issues existed know I can able to download and extract properly.
Regards,
Lakshmanan
2023-07-05 4:49 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter