2023-08-30 10:40 PM - edited 2023-08-30 10:53 PM
a)
On windows 11 with 2 screen the cubemonitor power v1.2.1 starts on one screen with the size way bigger than the screen. I have to resize the windows on the left outer edge -> height shrink automatically to match screen size -> then can move the whole window further left (on the left screen) to get to the right edge of the window -> then can make the window smaller to fit on one screen.
It would be good if the cubemonitor power v1.2.1 would start completely visible on one screen.
b)
exporting as csv is really slow and the cubemonitor power v1.2.1 becomes partly unresponsive . this is not a problem of the PC (64GB ram, some good 2th CPU, SSD).
I would assume that to be exported data is converted into a list (many small allocations) before handing it it to the csv writer - but that may be wrong. Anyway writing the csv should be way faster.
c)
it would be great to be able
a smaller improvement would be
as they show up in screenshots of the graph and legend area (screenshots necessary as no png export exists)
d)
when the select board ..... buttons would be moved in the logo line (there is lots of space left) as well as the accquisition and ulp bench tabs there would be more room for the graph.
btw. the logo line has
The page you are trying to access was not found. Please check your URL for typos and try again.
maybe put all these icon links into a help/about menu where also the documentation can be linked ?