cancel
Showing results for 
Search instead for 
Did you mean: 

LPM01A cannot connect to STM32CubeMonitor-Power

ADing.1
Associate II

I downloaded Cube Power Monitor and am trying to use it to connect to the LPM01A. I have downloaded and installed the W8 version of the virtual com port driver.

I can select the board in the drop down menu, but when I hit "Take Control", a dialog box pops up with the message `error pwr get`. When I hit okay, another pops up with the message `Get current range command failed` with another message below it `ERROR TIMEOUT`. Hitting ok again gives yet another dialog box with the message `Board has been released due to connection issue. Please unplug and plug the board`.

I've tried unplugging and plugging it back in and the same thing happens. I am currently on Windows 11, but I've tried on a different windows 10 machine and the result was exactly the same.

Any help would be appreciated.

Please also take a look at my other question for something that might be related... having lots of issues with this board so far...

11 REPLIES 11

Same for me. v1.2.0 kept throwing error. When I used 1.1.1 of graphical tool then it worked. ST never works straightaway out of the box. 

Richard.Chvr
ST Employee

Hello @PPa

Can you give more details about the STM32PowerMonitor errors.

Which version of STM32-LPM01-XN firmware are you using? You may updated in following link.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.