cancel
Showing results for 
Search instead for 
Did you mean: 

How to transfer mass data for STM-Studio using ST-LINK v2/v3

smiya.2
Associate II

I want to get mass data and display all these data on STM-Studio without delay.

but, Using default setting [acquisition rate is Maximum, Select "Display all data"] ,

I can get and display mass data with delay.

To get/display mass data without delay, Waht do you recomend for me ?

  1. I will try to modification the STM-Studio that was made by Java .
  2. I will try to modification the ST-LINK. I connect a external RAM to ST-LINK not to overflow RAM and not to delay

Are these charanges good idea ?

please hint for me.

thank you.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hi @Community member​ ,

New solution to replace STM-Studio is STM32CubeMonitor.

Some of the offered features:

  • Graphical flow-based editor with no programming needed to build dashboards
  • Connects to any STM32 device via ST-LINK (SWD or JTAG protocols)
  • Reads and writes variables on-the-fly from and to the RAM in real time while the target application is running
  • Direct acquisition mode or snapshot mode
  • Enables to log data into a file and replay for exhaustive analysis
  • Multi-probe support to monitor multiple targets simultaneously
  • ...

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3

Perhaps architect a solution using USB directly (STM32 to PC) that off-boards the volume of data you have?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for replying.

I can't use USB peripheral in my project.....

but , that is good idea.

Do you have the others idea ?

Amel NASRI
ST Employee

Hi @Community member​ ,

New solution to replace STM-Studio is STM32CubeMonitor.

Some of the offered features:

  • Graphical flow-based editor with no programming needed to build dashboards
  • Connects to any STM32 device via ST-LINK (SWD or JTAG protocols)
  • Reads and writes variables on-the-fly from and to the RAM in real time while the target application is running
  • Direct acquisition mode or snapshot mode
  • Enables to log data into a file and replay for exhaustive analysis
  • Multi-probe support to monitor multiple targets simultaneously
  • ...

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.