2024-12-06 4:41 AM - edited 2024-12-06 4:42 AM
Hallo,
I am saving the log files of the chart in the CUBEMonitor software. I read certain values from the MCU through Cube Monitor and save them as .CSV. However I've noticed that the first file I save after opening the software does start from 0 seconds. In case I stop the data acquisition and clear the chart and start it again. A new log file is created with advanced time i.e. although the chart does show the time scale to be from 0 seconds.
This problem doesn't occur if I restart the software, but it is tedious everytime to restart the software. Is there a way I can reset the time for every acquisition made?
Thanks
Solved! Go to Solution.
2024-12-10 12:20 AM
Hello @draco
The time of the logs are set to zero for the first log element after starting the tool.
The exact behavior is :Launch tool or deploy flow, then start acquisition -> the log timestamp is set to zero when the first data is stored in the log file. The timestamp will never be reset after. (until tool restart or new deploy)
For the graph, it is reset at startup or when a "clear" message is received (topic="clear"). But the "clear" message is not managed by processing node, so timing is reset only at launch or "deploy"
One workaround is to re-deploy the flow to reset the log counter. You may have to move an element in the flow, and then you can click on deploy. This is faster than restarting the complete software.
I am discussing within CubeMonitor team on how to improve for long term. There could be different solutions :
@draco : would it solve your point ?
Question for everyone : what would be your preferred option ? Would it be an interesting improvement for your use cases ?
Best regards
Stephane
2024-12-10 12:20 AM
Hello @draco
The time of the logs are set to zero for the first log element after starting the tool.
The exact behavior is :Launch tool or deploy flow, then start acquisition -> the log timestamp is set to zero when the first data is stored in the log file. The timestamp will never be reset after. (until tool restart or new deploy)
For the graph, it is reset at startup or when a "clear" message is received (topic="clear"). But the "clear" message is not managed by processing node, so timing is reset only at launch or "deploy"
One workaround is to re-deploy the flow to reset the log counter. You may have to move an element in the flow, and then you can click on deploy. This is faster than restarting the complete software.
I am discussing within CubeMonitor team on how to improve for long term. There could be different solutions :
@draco : would it solve your point ?
Question for everyone : what would be your preferred option ? Would it be an interesting improvement for your use cases ?
Best regards
Stephane
2024-12-10 12:48 AM
I think that solutions provided will work.
The option to restart the timer at 0 at chart and logFile would be a great idea as sometimes in past I did have certian measurements that I ran although the data was being pooled all the time.
Nevertheless, more options does provide flexibility to other use cases and thanks for the hint of re-deploying the flow. That will work for now!
Best regards,
Melwin