2023-01-26 11:09 PM
The code is a basic blinking LED and a free counter variable. The code runs well on the board. The list of variables is ok in STM32CubeMonitor.Thank you
2023-01-27 1:04 AM
Strange. Nothing at debug 1? Simplify your flow for debugging, e.g. remove BP bleu node.
hth
KnarfB
2023-01-27 2:02 AM
I already did it without success !! I tried aswell with only on chart and it does'nt works
No message at debug to.
2023-02-16 6:42 AM
Hello
For sure BP bleu single value node can be removed and ST Chart linked directly to processing node. Can't see the variable you're monitoring in the Monitor-2 screenshot. Can you share a bit more informations about elf and flow?