2024-07-17 8:54 PM - last edited on 2024-07-18 12:43 AM by mƎALLEm
安装Cubemonitor后,许多组件无法正常工作。我不知道为什么。我的安装环境有问题吗?但是我已经搜索了一些信息,我已经安装了JRE环境;仍将发生以下错误;
2024-07-18 12:40 AM
Hello @Pixrig and welcome to the community.
Please use English language to post in this international community? So you will maximize your chance to get an answer.
Thank you for your understanding.
Translation:
After installing Cubemonitor, many components cannot work properly. I don't know why. Is there something wrong with my installation environment? But I have searched for some information, I have installed the JRE environment; the following error will still occur
2024-07-18 1:24 AM
Hello
@Pixrig can you provide more details about your configuration ?
- What OS and version are you using ?
- Which version of the tool are you installing ?
- Have you already installed another version previously ? was it working ?
- Do you see some error if you start the tool in command line ?
thanks
To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
2024-09-24 2:55 AM
Hello
@Pixrig : can you check this post : https://community.st.com/t5/stm32cubemonitor-mcus/cubemonitor-acquitions-installing/m-p/660215/highlight/true#M1166
It looks similar, the workaround may be good for you.