cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE for OSX for MP1

Sindel
Associate

Is it possible to use the CubeIDE on OSX for debugging firmware for STM32MP1?

The interface is lacking some features and the debugging configuration is completely different.

Also I can't manage to make it work.

Here is what shows up when I launch Debug Configurations:

0693W00000ANb7ZQAT.png

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Cartu38 OpenDev
Lead II

As far as I'm aware STM32MP1 is not MacOS supported if debug.

Quite old post ... is it still valid ? See https://community.st.com/s/question/0D50X0000BxxoQSSQY/the-stm32cubeide-v110-hasnt-load-image-option-on-macos

Sindel
Associate

Thanks, I searched for OSX but it did not produce any result. Too bad that there is no support.

Compare a Linux install vs. MacOS one ... some debug components are lacking