2024-06-27 9:33 PM
Good evening,
Could you help me install the x-cube-cryptolib library in STM32CubeIDE? I have tried everything and I still can't install it correctly. I would greatly appreciate your help.
Solved! Go to Solution.
2024-06-27 9:43 PM
Hello @Zero-96 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to follow this article. It should be helpful.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-27 9:43 PM
Hello @Zero-96 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to follow this article. It should be helpful.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-30 12:59 PM
Hello, thank you for responding! I followed all the steps, but when I try to include the library with #include "crypto.h", I get an error. I am not sure if it needs to be called differently.