cancel
Showing results for 
Search instead for 
Did you mean: 

Which command for compiling only specific memory address (area in linker script)

Exit0815
Senior

Hello,

i have "splitted" the memory into several parts using the linker script.

Now i want to compile only one part to just upload that area.

They are splitted correct, so that an erase of one area will not touch the other areas.

i.e. external memory:

Area1 (r) : ORIGIN = 0x90000000, LENGTH = 2048K

Area2 (r) : ORIGIN = 0x90200000, LENGTH = 2048K

Now i just want to compile the Area2 that i have a file which only contains the Data from 0x90200000 to 0x903FFFFF

I hope that is possible.

Thank you very much.

0 REPLIES 0