Skip to main content
Brad Stewart
Associate II
February 7, 2021
Question

Where is the Discovery demo software that runs on CubeIDE????

  • February 7, 2021
  • 2 replies
  • 863 views

I have the latest STM32F407G-DISC1 board Rev D.

The software demos you download are not supported by CubeIDE.  The applications notes do not reference CubeIDE. (UM1467)

STM32F4-Discovery_FW_V1.1.0.zip is the name of the demo files.

I tried to import examples into my work bench using File-->Import-->general-->Existing Projects into Workspace.

None of the examples will compile. There are path issues. It's looking for the CMSIS library in C:\ Libraries\CMSIS which were not installed there by CubeIDE.

So what do I do? It seems I should be able to build the demos using the CubeIDE.

By the way, I am able to create new projects using CubeMX, but I really don't want to re-invent the wheel.

This topic has been closed for replies.

2 replies

Pavel A.
February 8, 2021

Please import the example projects as explained in the CubeIDE user manual.

Import-->Existing Projects into Workspace isn't expected to work, this action can import only projects already in CubeIDE format. it will not convert from other formats.

-- pa

Tesla DeLorean
Guru
February 8, 2021

It is probably old enough to be using SPL

For HAL examples, look under the CubeF4 repository trees for the board, and applications/demos

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..