cancel
Showing results for 
Search instead for 
Did you mean: 

USBX improper code generation

WDobb.1
Associate II

After editing the .IOC file, the code generator will mess up the app_usbx_device.c\MX_USBX_Device_Init() function by placing the code

if (ux_device_stack_initialize(...)

right after the variable declarations at the top of the function.

Typically, that function call should be around line 151 after 6 other function calls initialize all the pointer variables.

The end result is 8 compile warnings about using uninitialized variables.

Attempts to wrap the stack initialization in /* USER CODE BEGIN MX_USBX_Device_Init0 */ don't work, and the code generator will just move it to the top of the file anyway.

What is the work-around for this?

STM32H562VGTx

STM32CubeMX 6.12.0

STM32CubeIDE 1.16.0

 

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @WDobb.1 ,

First let me thank you for posting and welcome to the ST Community.

For more investigation, I suggest please that you provide the Ioc.File.

Thanks.

Mahmoud

 

The ioc file is attached.