2019-06-28 1:36 AM
Hello support team ,
i have tried to Update Stm32CubeIDE on update site
http://sw-center.st.com/stm32cubeide/updatesite1
i have a systematic issue
An error occurred while collecting items to be installed
session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,org.apache.httpcomponents.httpclient.win,4.5.6.v20190213-1947
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.core,1.7.6.v20190415-1216
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.core.win32,1.7.6.v20190415-1216
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.help.ui,1.7.6.v20190415-1216
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.ui,1.7.6.v20190416-1746
No repository found containing: osgi.bundle,org.eclipse.epp.mpc.ui.css,1.7.6.v20190415-1216
No repository found containing: org.eclipse.update.feature,org.eclipse.epp.mpc,1.7.6.v20190416-1746
Best regards
Erwan
2019-07-03 7:18 AM
Is this for version 1.0.0 or 1.0.1?
Do you use a proxy? If so make sure you have input the correct settings, reload might help to validate them.
You can try to clear your p2 cache by deleting this following folder. After you've doen that you can go to Help > Check for updates:
INSTALL_LOCATION\STM32CubeIDE\p2\org.eclipse.equinox.p2.repository\cache
2019-07-18 1:27 AM
I'm seeing this too on CubeIDE 1.0.0
My home install was done later and that has just updated successfully. I guess I need to reinstall over the 1.0.0 with a new download?
2019-07-18 2:12 AM
Hello , the problem is Solved ..
Thank you for tour support
2019-07-18 2:23 AM
I can confirm, 1.0.2 appears to access the update dialogue correctly.
2019-07-28 11:54 PM
How did you solve this problem?
In this tread I see 3 recommendations:
Which one did you use?
2019-07-29 1:25 AM
I downloaded 1.0.2, which solved the issue
2019-07-29 1:29 AM
Thank you!
2019-10-16 7:11 AM
clearing cache is solved my problem
2020-10-15 9:27 AM
You can try to setup with you site or any website that hosted online. See some best result and examples.