Question
Unable to program Nucleo-64 using Mac/USB, cubeIDE gives "No ST-LINK detected" message.
I'm trying to program a Nucleo-64 (STM32G070RBT6) using:
- CubeIDE version 1.11.0, project is set up with the target as the above board.
- MacBook Air, M1 2020
- micro USB cable connected to board and the Mac
Things I've tried:
- different USB cables
- different USB ports on the Mac
- Tried programming another (identical) Nucleo-64 board.
What I see on the board:
- COM LED is red
- LD3 LED is on (not flashing)
- LD4 LED is on/flashing.
I press on the 'Play' or 'Debug' buttons in CubeIDE to try to upload my program, but it always gives the "No ST-LINK detected" message, and the board is not programmed.
Am I missing something? Do I need a USB driver for Mac? I did find a USB driver on the ST website, but it is only for Windows.
Any help or suggestions are welcome, thank you!