2023-11-02 7:59 AM
Hello,
I am trying to import a project from Atollic into STM32CubeIDE. I follow the instructions in UM2578 but when I click the "Finish" button nothing happens. No confirmation box appears and no new files are generated in the project folder. Any ideas of what may be causing this?
2023-11-02 9:35 AM
Hello @Xortan and welcome to the community,
Could you, please, provide which OS and the firmware used for this project .
Thanks,
Rim.
2023-11-02 9:42 AM
I am using Windows 10. I am not sure if I can provide the firmware as its proprietary.
I was able to kind of do an import, but the project was in a different location than the selected workspace.
2023-11-02 9:49 AM
So to kind of clarify what I am seeing, I am able to open a project if its not in my selected workspace.
My workspace is set to C:\Users\xxx\Documents\STM Workspace
If I place my Atollic project files in a different directory and open the project file, it apparently does the import.
I tried to move the files after it did an import into my workspace, but I cannot open any projects that are in C:\Users\xxx\Documents\STM Workspace
2023-11-02 3:01 PM
>C:\Users\xxx\Documents\STM Workspace
Choose another directory name, without spaces. Proven recipe for trouble.