cancel
Showing results for 
Search instead for 
Did you mean: 

Timer callback function created by RTOS does not working .

YDOOY.1
Associate II

I am a biginner of STM32CubeIDE.

I made an example which run timer function with STM32cubeIDE.

But the timer callback function is not run, Even though osTimerStart() is called in StartDefaultTask() function. What should I change?

Thank you in advance.

Here is my source code..

int main(void)

{

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_ADC1_Init();

 MX_DFSDM1_Init();

 MX_ETH_Init();

 MX_FMC_Init();

 MX_I2C1_Init();

 MX_LTDC_Init();

 MX_QUADSPI_Init();

 MX_SAI1_Init();

 MX_SDMMC1_SD_Init();

 MX_USART1_UART_Init();

 MX_USB_OTG_FS_PCD_Init();

 MX_USB_OTG_HS_PCD_Init();

 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Init scheduler */

 osKernelInitialize();

/* creation of myTimer01 */

 myTimer01Handle = osTimerNew(Callback01, osTimerPeriodic, NULL, &myTimer01_attributes);

 /* creation of myTimer02 */

 myTimer02Handle = osTimerNew(Callback02, osTimerPeriodic, NULL, &myTimer02_attributes);

defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);

 /* USER CODE BEGIN RTOS_THREADS */

 /* add threads, ... */

 /* USER CODE END RTOS_THREADS */

 /* Start scheduler */

 osKernelStart();

 /* We should never get here as control is now taken by the scheduler */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

 }

} // End of main()

...

..

.

/* USER CODE END Header_StartDefaultTask */

void StartDefaultTask(void *argument)

{

 /* USER CODE BEGIN 5 */

osDelay(10);

osTimerStart(myTimer01Handle, 20);

osDelay(10);

osTimerStart(myTimer02Handle, 20);

 /* Infinite loop */

 for(;;)

 {

 if(osTimerIsRunning(myTimer01Handle) ) {

printf(" Tmr callback01 is running ....\n\r");

}

else {

printf(" Tmr Callback01 is not working... Re-Start Timer....\n\r");

osTimerStart(DGP_Tx_TMRHandle, 20);

}

osDelay(1000);

if(osTimerIsRunning(myTimer02Handle) ) {

printf(" Tmr is Callback02 running ....\n\r");

}

 }

 /* USER CODE END 5 */

}

/* Callback01 function */

void Callback01(void *argument)

{

 /* USER CODE BEGIN Callback01 */

while(1) {

printf(" Timer Callback 01 is running .....\n\r");

osDelay(100);

}

 /* USER CODE END Callback01 */

}

/* Callback02 function */

void Callback02(void *argument)

{

 /* USER CODE BEGIN Callback02 */

while(1) {

printf(" Timer Callback 02 is running .....\n\r");

osDelay(100);

}

 /* USER CODE END Callback02 */

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0