cancel
Showing results for 
Search instead for 
Did you mean: 

Theme can not be switched on KDE Linux

user7
Associate II

I'm using STM32CubeIDE (Linux generic version) on Linux Mint Debian Edition, KDE Window Manager. 

When starting it as normal user the Themin is not working (Preferences-General-Appearance). The window has a dark theme (the one I choose in my KDE preferences). But I would like to use the default light theme. 

The only way to do this is by running STM32CubeIDE with sudo. Is this expected or is there a workaround? 

 

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
user7
Associate II

I found the solution for this. You have to add a line to the startup script "stm32cubeide_wayland" which is located in the stm32cubeide_x.xx.x folder

Before the last line that starts cubeide add the line:

export GTK_THEME=Adwaita

Would be nice if this could be added by ST per default into this script. 

 

View solution in original post

1 REPLY 1
user7
Associate II

I found the solution for this. You have to add a line to the startup script "stm32cubeide_wayland" which is located in the stm32cubeide_x.xx.x folder

Before the last line that starts cubeide add the line:

export GTK_THEME=Adwaita

Would be nice if this could be added by ST per default into this script.