2019-06-19 12:08 AM
2019-06-19 7:25 AM
If you are behind a proxy make sure that your settings are correctly set, the reload button may help to validate them.
Otherwise I suggest you to clear your p2 cache by deleting the following folder, and try again Help > Check for updates:
INSTALL_LOCATION\STM32CubeIDE\p2\org.eclipse.equinox.p2.repository\cache
2019-06-19 1:05 AM
We're investigating it right now, I'll update you once I know more.
2019-06-19 1:26 AM
Thanks Markus
2019-06-19 7:02 AM
Could you provide more details on the usecase that conduct to this 404 error?
Note that this site is not supposed to display something with a web browser, I also get a 404 error in Chrome even if update-site works like a charm through STM32CubeIDE.
What happen if you press the reload button of STM32CubeIDE repository site?
2019-06-19 7:17 AM
Hi Julien,
This is actually occurring in the STMCUBEIDE when I go to Help> Check for updates.
I get this error:-
Thanks James
2019-06-19 7:23 AM
Hi Julien,
When I go into the list of available sites and reload i get this:-
2019-06-19 7:25 AM
If you are behind a proxy make sure that your settings are correctly set, the reload button may help to validate them.
Otherwise I suggest you to clear your p2 cache by deleting the following folder, and try again Help > Check for updates:
INSTALL_LOCATION\STM32CubeIDE\p2\org.eclipse.equinox.p2.repository\cache
2019-06-19 7:29 AM
Definitively clearing you cache will solve the issue.
2019-06-19 7:34 AM
Hi Julien,
I deleted the files from the Cache and that seems to have done the trick.
Thank you for your help.
Cheers
James
2019-06-19 7:44 AM
Great !
You're welcome, feel free to mark the topic as resolved.
Julien