Different startup files for STM32F373VCTX if choosen STM32Cube or Empty as targeted Project Type
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-06-20 12:19 AM
I use STMCubeID V1.0.0
I realised that there is a difference of the names in the vector table for the can irqhandlers.
If I choose STM32Cube as target, I get a startup_stm32f373vctx.s file with the names:
- CAN_RX0_IRQHandler
- CAN_RX1_IRQHandler
If I choose Empty as target, I get this names:
- CAN_RXD_IRQHandler
- CAN_RXI_IRQHandler
Why is this difference and for waht do the letters "0"/"1" and "D"/"I" stand for?
Labels:
- Labels:
-
CAN
-
STM32CubeIDE
-
STM32F3 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0