cancel
Showing results for 
Search instead for 
Did you mean: 

Target selection: STM32 target or STM32Cube example selection is required

Dabbo
Associate III

Running on Ubuntu

STM32CubeIDE

Version: 1.13.2

Build: 18220_20230914_1601 (UTC).

Fresh installation but just getting blank page saying "Target selection: STM32 target or STM32Cube example selection is required".

I've:

1. Checked for target selector device database updates

2. Checked for Embedded Software Packages Updates

3. Managed Embedded Software Packages and installed latest package for STMG0

Rebooted etc, but still getting this message and can't get past.

PS: STM32CubeIDE runs fine on Windows 11 connected to target board (Nucleo-64 G071RB)

26 REPLIES 26
ilovethissoftware
Associate

I ran into a problem today where the program got stuck on the splash screen and would not start. This was solved my deleting the .metadata folder in my workspace. This is a hidden folder, as indicated by the dot, and you can see it in GUI file manager by Settings -> Show hidden files (Ctrl + H). In terminal you would type ls -a to list all folders including hidden ones, and rm -rf .metadata to delete it.

Oskar_H
Senior

Hello,

yes this hidden directory contains very sensitive data that sometimes make the whole thing unstable.

I had to delete some parts of it regularly to overcome issues at start.

Please someone at ST can confirm this will be fixed ?

And I repeat, there is no mention in the documentation about the specific install script for Wayland. Someone at ST can confirm this will be documented ?

Oskar_H
Senior

Any update about this topic ?

This fixed my issue on Ubuntu 22.04.4 LTS running:

STM32CubeIDE
Version: 1.15.0
Build: 20695_20240315_1429 (UTC)
OS: Linux, v.6.5.0-27-generic, x86_64 / gtk 3.24.33
Java vendor: Eclipse Adoptium
Java runtime version: 17.0.8.1+1
Java version: 17.0.8.1

Doom
Associate

I use "stm32cubeide_wayland" instead of "stm32cubeide", and it works

(linux installation (1.16.0) on an Ubuntu 24.04LTS)

It's 2025 and it's still not working.

"Wayland being well known to have a lot of issues" is not an excuse; I've been using Wayland for more than 5 years, and 95% of the software runs under Wayland really well.

This also worked for me as 2026-05-07

Arch Linux (BTW) 7.3.1

KDE plasma 6.6.4 - wayland

openjdk 26.0.1 2026-04-21
OpenJDK Runtime Environment (build 26.0.1)
OpenJDK 64-Bit Server VM (build 26.0.1, mixed mode, sharing)

stm32cubeide version 1.19.0 (yes it's not the most recent version)