STM32WB5MM OTA with BLE custom template
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-09 5:52 AM
Hello,
I am using the STM32WB5MM with BLE Custom Template configuration, and I need to perform an OTA firmware update for my application. I have watched the "Getting started" series with this MCU, especially the video available at https://www.youtube.com/watch?v=mRzZOa3jmuM. However, in those videos, the board used is the STM32WB55, which is not compatible with my STM32WB5MM. I am currently working with the STEVAL-PROTEUS1 evaluation board.
I understand that I need to load the "BLE_OTA" example first at a specific address (0x08000000), and then load my application code at a different address (0x08007000). Since the MCUs are different, I couldn't follow the steps exactly as shown in the video for debugging this section (6:40 - 8:10 in the video).
Therefore, I manually modified the linker script stm32wb5mmghx_flash.ld so that the application code starts from 0x08007000, making it compatible with OTA configuration. However, I couldn't replace the system_stm32wbxx.c file for the same reason of incompatibility.
Now, I have a couple of questions:
Is it possible to activate the OTA configuration using CubeMX instead of manually changing and debugging it?
Do you have any alternative solutions for OTA configuration when working with a different MCU than the STM32WB55?
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-10 4:51 AM
Hello @DanielAbramov ,
Maybe the STM32Wiki MCU can help you. https://wiki.st.com/stm32mcu/wiki/Category:Bluetooth_Low_Energy
There are articles on FUOTA for STM32WB and WBA.
https://wiki.st.com/stm32mcu/wiki/Category:STM32WBA_FUOTA
https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_Fast_FUOTA
Best Regards
Michael
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-07-10 5:02 AM
Hellow @Michael E ,
I have read the articles you mentioned. doe the example of BLE_OTA is compatible with stm32wb5mm?
Best Regards
Daniel