2021-03-14 11:10 AM
I have a stm32L476G-DISCO.
trying to get this simple blink led program working.
CODE:
while (1)
{
HAL_GPIO_TogglePin( LD_G_GPIO_Port, LD_G_Pin );
//(LD_R_Pin);
HAL_Delay(2000);
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */BUILD SUCCESS:
14:08:04 **** Incremental Build of configuration Debug for project Lab2-Kava ****
make -j8 all
arm-none-eabi-size Lab2-Kava.elf
text data bss dec hex filename
39640 152 4064 43856 ab50 Lab2-Kava.elf
Finished building: default.size.stdout
14:08:05 Build Finished. 0 errors, 0 warnings. (took 396ms)UPLOAD ATTEMPT:
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down...Really baffled why its not uploading. ST made me upload the firmware on the board.
2021-03-15 9:00 AM
Hello @Kt.1,
Welcome to ST community :smiling_face_with_smiling_eyes:.
This a debugger problem. Please check the cable you are using and make sure that you have correctly configured the Debug Configuration and connected to the ST-Link on the board.
If you are using STM32CubeIDE, I recommend you checking the 3rd section of the STM32CubeIDE User Guide.
Chahinez.