2023-07-24 11:53 PM
Used STM32CubeIDE version: 1.12.0
Used driver library: STM32Cube_FW_U5_V1.2.0
I found a bug in the initialization of the LSI, when low-level drivers are used. The bug is located in the function SystemClock_Config(). Since the background domain access is not enabled before trying to enable the LSI, the loop which is waiting for the LSI to come up is never left.
...
LL_PWR_EnableBkUpAccess(); // <-- this line is missing in the generated code
LL_RCC_LSI_Enable();
/* Wait till LSI is ready */
while(LL_RCC_LSI_IsReady() != 1)
{
}
...
Solved! Go to Solution.
2023-07-26 1:43 AM - edited 2023-07-26 1:44 AM
Hello @SOfne.1
First let me thank you for posting.
Actually I tried to reproduce the issue mentioned above using STM32U575,CubeMX 6.9.0 and STM32CubeIDE 1.13.0 and this is what I got please have a look
"LL_PWR_EnableBkUpAccess()" does exist in the generated code.
Thx
Ghofrane
2023-07-26 1:43 AM - edited 2023-07-26 1:44 AM
Hello @SOfne.1
First let me thank you for posting.
Actually I tried to reproduce the issue mentioned above using STM32U575,CubeMX 6.9.0 and STM32CubeIDE 1.13.0 and this is what I got please have a look
"LL_PWR_EnableBkUpAccess()" does exist in the generated code.
Thx
Ghofrane
2023-07-26 1:56 AM
Hi Ghofrane,
the code you generated is OK.
Seems that the bug has already been fixed with STMCubeIDE 1.13.0.
(I currently use v1.12.0)
Thanks
Sebastian