2019-09-15 1:53 AM
So, I am learning stm32 mcus, using a nucleo f4 board.
Everything was working fine and now debug launch fails.
Actually, I was doing one debug, closed it and next debug session won't launch.
Atollic TrueSTUDIO does work with the same settings (st-link gdb server in the debugger settings).
CubeIDE works in linux.
Solved! Go to Solution.
2019-09-15 4:39 AM
Guys, avast antivirus deletes the st link server exe file. It is absolutely because of it.
I had to add an exception for the exe file.
2019-09-15 2:19 AM
After a few reinstalls, I noticed that when the error raises, in the folder plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.0.0.201904160814\tools\bin the st link server execbutable is missing.
On this fresh reinstall, I backed it up.
I'm using avast free antivirus, maybe it is giving me problems. The server is allowed in windows firewall.
2019-09-15 4:39 AM
Guys, avast antivirus deletes the st link server exe file. It is absolutely because of it.
I had to add an exception for the exe file.
2019-09-22 6:05 AM
I've got same problem and along with dedi1's way, finally got working set of st link with gdb.
Thanks dedi1 ;)
2020-05-02 5:50 AM
jjank, I'd just like to thank you for making this public. I banged my head against this for a long time before finding your explanation.
I'll report it to Avast as a false positive.
2020-05-02 7:37 AM
Just for the mention, my stlinkserver.exe was not down among the plugins as in your case - it was in
C:\Program Files (x86)\STMicroelectronics\stlink_server
I have set an Avast exception for the entire C:\Program Files (x86)\STMicroelectronics\*
and I've made a backup of it too. However, when I tried to make a backup of the entire C:\Program Files (x86)\STMicroelectronics folder,
I was unable to because Windows said that file names were too long for the destination folder.
Anyway, the stlink_server folder copied OK.
2020-08-22 11:35 AM
Thank you guys. The solution is perfect and working 100% percent.