2024-10-19 2:45 AM
Greetings!
The problem that I have is that Project Explorer in STM32CubeIDE shows error symbol on the name of the project that I have but the when building the project, console window shows 0 errors. However I have ran the .elf file on Hardware without problems but I still worry about this error symbol.
2024-10-19 2:52 AM
Hello @Ajnyhaa
I suggest you just to click on the name and select the option clean to clean your project. After that, rebuild your project. That should eliminate the error symbole.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-19 6:04 AM - edited 2024-10-19 6:05 AM
@STTwo-32 Thank for reply. Unfortunately I have cleaned and rebuilt project many times but the issue not fixed.
2024-10-19 6:07 AM
If you are not using the V1.16.1. please update your CubeIDE. If so, please upload your project here.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.