2023-11-06 4:11 AM
Hello,
i am using STM32CubeIDE with SWV and want to change the color and the thickness of data lines in the SWV data trace timeline graph. Is it possible to change it? If yes, how can i do it?
BR
Heimo
2023-11-07 7:27 AM
Hello @ledi007 and welcome to the community!
Unfortunally there is no option to change the color and the thickness of data lines in the SWV data trace timeline graph in STM32CubeIDE
the appearance and color of data lines in trace graphs are often predefined by the tool.
Thank you,
Souhaib