cancel
Showing results for 
Search instead for 
Did you mean: 

error "no ST Link detected"

zanna989
Associate II

hi everyone, idk if this problem was already reported but i didn't find anything that helped me solving my problem.

i'm using the board B-L475EIOT01A and everytime i try to debug in my STM IDE it tells "no ST Link detected".

can someone pls tell me step-by-step how to solve this problem?

can it be that my pc doesn't see the board?

thanks

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6

You'd need to see the board and an ST-LINK in Device Manager. You'd need the right driver, a suitable data cable, and plug into the correct USB port. Check the board provides an ST-LINK, and not an external SWD/JTAG pod.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
zanna989
Associate II

so it's possible that the data cable could be the problem
actually I went to look at Device Manager and it seems that the board is not seen by the PC

also how can i check that the board is providing an ST-LINK
sorry if my questions are trivial but i'm a beginner

ST-LINK is on-board via connector in North East top edge. Make sure you have a good cable, not a power-only charger cable.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

i think everything is working properly, also the cable is the one that my university gave to me.

i read that the problem could be the firmware version, could it be?

idk how to do the update

The STM32 Cube Programmer firmware update for the ST-LINK still needs to see the device.

Work with someone who knows how to run Windows.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
zanna989
Associate II

ok thanks