cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE: Application Strucutre is stuck to Advanced

Romder
Associate

Hello everyone!

 

Everything is in the title. I'm not sure at which point I changed the structure to Advanced (probably when trying to debug), but I ended up with a massive main.c file. Now, the Application Structure cannot be changed. Do I need to remake the project from scratch, or is there a way to revert to basic?

 

Thanks in advance.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

From looking around, the project structure is meant to be fixed on project creation, but you can edit it manually within the IOC file in a text editor.

Solved: STM32CubeMX 6.13.0 - Application Structure is Basi... - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

From looking around, the project structure is meant to be fixed on project creation, but you can edit it manually within the IOC file in a text editor.

Solved: STM32CubeMX 6.13.0 - Application Structure is Basi... - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Evangelist III

I ended up with a massive main.c

??? Do you actually mean, create separate c & h files for each peripheral?

PavelA_0-1741920890881.png

 

I apologize, this was indeed a separate issue..