2024-11-29 1:14 AM
Dear all,
when I press Install button in the Toolchain Manager of the 1.17.0 CubeIDE it hangs after opening the subsequent dialog. I cannot close this dialog with neither mouse nor ESC key, need to terminate the task.
Regards,
Dmitry
2024-11-29 1:22 AM
Hello @DmitryR
Could you provide more information about your OS and environment where you installed CubeIDE?
KR,
Souhaib
2024-11-30 1:59 AM
Hi @Souhaib MAZHOUD ,
Thank you for your attention. My OS is Windows 10 version 22H2 build 19045.5131. System has 16Gb RAM, Typically 40% of it is free when STM32CubeIDE is running. Seems that it stucks on printing a message that is marked red on the image attached.
Regards,
Dmitry
2024-12-02 5:40 AM
Hello @DmitryR
Actually, I am not able to reproduce the issue with the same OS environment as yours. The toolchain manager is working correctly and I successfully installed toolchains with CubeIDE 1.17.0.
I suggest reinstalling CubeIDE and trying again!
KR, Souhaib
2024-12-02 10:07 AM
Hi @Souhaib MAZHOUD ,
thank you for your attention. After new installation of the STM32CubeIDEI have successfully installed the toolchain. But there is a problem still. When I click "next" on the dialog I have already posted I get nearly the same dialog. If I click "finish" there it returns to Toolchain Manager and nothing happens. The problem is that I should wait about 15 seconds on the second dialog. Then I receive (without clicking anything) a dialog where I must choose what sources I trust, and after that new toolchain is installed.
Regards,
Dmitry
2025-01-22 4:56 PM
Exact same issue, except I do not get the option to select trusted sources.
It takes 10 minutes to verify toolchains upon starting toolchain manager.
Also it shows a previous toolchain as uninstalled even though I can clearly see it on the drive along with the newer toolchain. This new toolchain is breaking all my existing projects and making the binary crash after upgrading to the latest IDE. I assume the toolchain change is the reason. How do you add the existing on e back in, or make this toolchain manager actually install something? All my projects are now dead due to IDE upgrade, desperately needs fixing.
2025-01-22 5:49 PM
I have reinstalled CUBEIDE but get exactly the same result.
after clicking the finish button there is no response and does not download anything.
Edition Windows 11 Home
Version 24H2
Installed on 18/12/2024
OS build 26100.2894
Experience Windows Feature Experience Pack 1000.26100.36.0
Please help, work has stalled on many projects due to incorrect gnu toolchain!
2025-01-22 5:56 PM
I finally got the trust window to display aftre many minutes, but still did not download and displays Installing software 13% and never moves
2025-01-22 6:10 PM
I finally after waiting an hour had the second trust window pop up and finally install it.
Please fix this! I was searching for an older version of CUBEIDE but see those have been removed as well.
Please fix this atrocious software and allow users to go back to old versions when you break it.