2023-11-28 5:27 AM - edited 2023-11-28 5:31 AM
Hello. I have the following problem. When I enable flto optimization in a (freshly generated) project, several dozen warnings appear during compilation.
Sample warnings:
Drivers/STM32L4xx_HAL_Driver/Src/subdir.mk:88: warning: pattern recipe did not update peer target 'Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal_cortex.su'.
Drivers/STM32L4xx_HAL_Driver/Src/subdir.mk:88: warning: pattern recipe did not update peer target 'Drivers/STM32L4xx_HAL_Driver/Src/stm32l4xx_hal.cyclo'.
This problem was not present on the previous version 1.13.2
How to solve this problem?
2023-11-28 6:37 AM
Hello @SKape
First let me thank you for posting.
Could you please provide the exact parameter settings that you used in order to reproduce your issue.
I will be waiting for your feedback.
Thx
Souhaib
2023-11-28 9:19 PM
I'm generating a new one STM32 project using Wizard, for example for STM32F103CB.
In the project settings, in the compiler options (Tool Settings/MCU GCC Compiler/Miscellaneous/Other flags), I add the -flto option.
I add the same to the linker options. And that's all.
34 warnings appear during compilation.
2023-11-30 12:09 AM
@Souhaib MAZHOUD Were you able to reproduce the issue?
2023-11-30 12:37 AM
Hello @SKape
Yes, this problem is reproduced in my side, I will check it internally and get back to you as soon as possible.
Thank you
2023-12-05 4:14 AM
Hello again,
After check, this issue is reported internally to our team (Internal ticket number: 167964) and this will be fixed as soon as possible.
Thank you!
Souhaib
2023-12-05 10:06 AM
Having the same issue
2023-12-11 3:26 AM
I have also the same issue...
2023-12-12 11:19 PM
I also use the -flto flag, so I got the same warnings....
BR
Andreas
2024-01-01 6:03 AM
Hello,
i'd like to add, that i get the same problem (lots of "pattern recipe did not update peer target" from the build output, CubeIDE 1.14.0, STM32G474), but for a different reason (not using "-flto).
I use "-Wswitch-enum" for the whole project, but explicitly removed this setting for the "Driver" file tree.
Please also see here for a possible useful hint:
It seems this problem was introduced by version 4.4 of gnu-make.
So can i go back to pre-4.4 in CubeIDE, or is it hard-coded?
Thanks and BR,
Albert