cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube IDE 1.4.0 Device configuration tool deletes the project.

LWei.1
Associate II

When I use .ioc file to generate the codes, it delete the entire project folder (include git information). Looks like I lose all the commits I haven't pushed to github. WTH is that.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

There was an unfortunate bug in 1.4.0 that caused files to get deleted in certain cases. Might try updating to 1.4.2 to see if it's fixed.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

There was an unfortunate bug in 1.4.0 that caused files to get deleted in certain cases. Might try updating to 1.4.2 to see if it's fixed.

If you feel a post has answered your question, please click "Accept as Solution".
Imen.D
ST Employee

Hello @LW.2ei​ ,

This issue is fixed in the STM32CubeIDE v1.4.2, as mentionned in the STM32CubeIDE release note.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen