stm32 with simcom A7672S
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-20 10:03 PM
#include "main.h"
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#define GETCHAR_PROTOTYPE int __io_getchar(void)
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart2;
PUTCHAR_PROTOTYPE
{
HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
return ch;
}
GETCHAR_PROTOTYPE
{
uint8_t ch = 0;
__HAL_UART_CLEAR_OREFLAG(&huart2);
HAL_UART_Receive(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
return ch;
}
int id = 212200;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART2_UART_Init(void);
void parseCmd(char* command, int timeout);
int main(void)
{
setvbuf(stdin, NULL, _IONBF, 0);
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
HAL_GPIO_WritePin(Enable_key_GPIO_Port, Enable_key_Pin, GPIO_PIN_SET);
HAL_Delay(2000);
HAL_GPIO_WritePin(Power_key_GPIO_Port, Power_key_Pin, GPIO_PIN_RESET);
HAL_Delay(2000);
printf("Sending AT commands...\n");
while (1)
{
char strAT[50];
parseCmd("AT\r\n", 1000); //Check AT
parseCmd("ATE1\r\n", 1000);
parseCmd("AT+CSQ\r\n", 1000);
parseCmd("AT+CPIN?\r\n", 1000);
parseCmd("AT+CREG=1\r\n", 1000);
parseCmd("AT+CGREG?\r\n", 1000);
parseCmd("AT+CGATT=1\r\n", 1000);
parseCmd("AT+QIFGCNT=0\r\n", 1000);
parseCmd("AT+QICSGP=1,\"WWW\",\"\",\"\"\r\n", 1000);
parseCmd("AT+QIREGAPP\r\n", 1000);
parseCmd("AT+QIACT\r\n", 1000);
HAL_Delay(2000);
sprintf(strAT, "AT+QHTTPURL=%d,%d", str_len, 180);
//Serial.println(strAT);
printf("The string %s",strAT);
parseCmd(strAT, 1000);
parseCmd(json_1, 3000);
parseCmd("AT+QHTTPPOST=60", 3000);
parseCmd("AT+QHTTPREAD", 3000);
parseCmd("AT+QIDEACT", 1000);
void parseCmd(char* command, int timeout)
{
HAL_Delay(timeout);
char rxdata[300];
memset(rxdata, 0, sizeof(rxdata));
// Transmit command over UART1
HAL_UART_Transmit(&huart1, (uint8_t*)command, strlen(command), timeout);
// Receive response over UART1
HAL_UART_Receive(&huart1, (uint8_t *)rxdata, sizeof(rxdata), timeout);
// Transmit response over UART2
HAL_UART_Transmit(&huart2, (uint8_t *)rxdata, strlen((char *)rxdata), timeout);
}
OUTPUT:
10:29:51.329 -> AT
10:29:51.329 -> OK
10:29:53.295 -> ATE1
10:29:53.295 -> OK
10:29:54.323 -> AT
i am using the above AT commands in simcom A7672S ,i am unable to get the proper response from the simcom, may, i know what the issues i am facing, Guide me with the issues i am facing her and help me to sort out this issues
21 REPLIES 21
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-23 4:30 AM
no i dint send the AT+HTTPSEND, is their any command like that, using the AT command data sheet thier is no command like that
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-23 5:30 AM
Sorry, HTTPSEND was for 7672, Can you try AT+HTTPREAD and AT+HTTPHEAD , I am referring to
https://www.ktron.in/wp-content/uploads/2023/03/A76XX-Series_AT_Command_Manual_V1.06-4.pdf
but anyway please try to do the reading from UART_RECEIVE_IT, interrupt, so that you will not miss characters
If you feel a post has answered your question, please click "Accept as Solution".

- « Previous
- Next »