cancel
Showing results for 
Search instead for 
Did you mean: 

RE: STM32CubeIDE Bug: While using the Pinout & Configuration "tool tip" has too short of display timeout.

dcomer
Associate II

On macOS 12.3.2 (Monterey), placing the cursor over a yellow warning icon, and attempting to read the warning text is dismissed way to fast. This, obviously, is a timeout that should either not occur until the cursor move off the object, or extended to allow the user to read the warning. Can this be fixed.

The application is fantastic, but this is a bug that should be addressed IMHO.

Thanks,

Dave

0 REPLIES 0