Skip to main content
SMura.1
Visitor II
March 8, 2020
Question

Problems with STM32CUBEIDE- Nucleo H743ZI SD card interface using SDMMC

  • March 8, 2020
  • 0 replies
  • 581 views

Hi,

I am currently using the Nucleo H743ZI board to interface with an SD card to Read/Write some data. I am using SDMMC in 1 bit mode to achieve this. I wrote the generic code (given below) to perform the write function. While using STM32CUBEIDE V1.2.0 however, I am unable to write data onto the SD card. During debugging I paused the program to check where the problem occurs. It appears as if the program never comes out of the f_mount function and is stuck there. Do you have any thoughts on this?

CODE:

FATFS myFATAFS;

FIL myFILE;

UINT testByte;

 if(f_mount(&myFATAFS, SD_Path, 1)== FR_OK)

   {

  HAL_GPIO_TogglePin(GPIOB,GPIO_PIN_7);

    char myPath[]="WRITE1.TXT\0";

    f_open(&myFILE, myPath, FA_WRITE | FA_CREATE_ALWAYS);

    char myData[] = "Hello World\0";

    f_write(&myFILE, myData, sizeof(myData), &testByte);

    f_close(&myFILE);

   }

I have seen other threads where this problem has been discussed to no real conclusion

Can you help me out with this?

This topic has been closed for replies.