2021-09-14 11:20 PM
I want to place a variable at a fixed address on my flash memory:
#define MYDEF "abcdefg"
const u8 MY_CHAR[] __attribute__((section(".ARM.__at_0x0blabla"))) = MYDEF;this works with KEIL IDE, but I switched to STM32CUBE IDE and it is not working. The mcu is an STM32F10
How do I have to change the attribute? Do I have also to change the linker script file ? This scares my...
Thanks
2021-09-15 12:32 AM
STM32CubeIDE uses a different toolchain to KEIL.
Its compiler is described at https://gcc.gnu.org/.
Its linker is described at https://sourceware.org/binutils/docs/ld/index.html.
2021-09-15 1:32 AM
So, I changed this to:
const u8 MY_CHAR[] __attribute__((section(".mySection"))) = MYDEF;and add this to .ld file:
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K
}
/* Sections */
SECTIONS
{
/* other placements follow here... */
.mySegment 0x8002000 : {KEEP(*(.mySection))}
/* The startup code into "FLASH" Rom type memory */
...and so onBut got compilation error if I put an address related to flash ( i.e. 0x8002000)
If I put 0x2000000 I got no error, what am I doing wrong ?
section .mySegment LMA [0000000008002000,000000000800200e] overlaps section .text LMA [00000000080001e8,000000000800c0cf]
2021-09-15 6:39 AM
The GCC linker isn't really set up to do this. You need to create a new section in memory and place the variable there, but it can't be in the middle of your flash.
It's easier to use a pointer and initialize manually.
2021-09-15 7:44 AM
Noobie question:
In this way also my .bin file will have this string at the address i want?
I want to put a string in a particular address i.e. : 0x8002000 ( so if I open the file with HxD it will show me this string at 0x8002000) is it possible to do with a pointer at compiling time ?
2021-09-15 8:05 AM
> I want to put a string in a particular address i.e. : 0x8002000 ( so if I open the file with HxD it will show me this string at 0x8002000) is it possible to do with a pointer at compiling time ?
No, it's not. You'd need to modify the linker to do that. But there's no easy way to place it at an absolute location within an existing memory section.
2021-09-15 9:39 AM
Does the executable code take more than 0x2000 bytes ? the linker error seems to indicate that the code goes beyond 0x08002000 and you try to force a constant to be at this address.
could you try to place the constant after the end of the code ? (way after 0x08002000).
2021-09-16 4:50 AM
> want to put a string in a particular address i.e. : 0x8002000
As apps grow larger and complex, where things are needs organising. That's what the linker command file is for.
Many details and options. Read the link I posted earlier about LD thoroughly.
This is a really dumbed-down example.
In the linker command file:
<snip>
MEMORY
{
<snip>
MY_FLASH_AREA (r) : ORIGIN = 0x8002000, LENGTH = 1K
}
SECTIONS
{
<snip>
MY_FLASH_AREA (NOLOAD) :
{
*(MY_FLASH_AREA)
} >MY_FLASH_AREA
}In your C source code:
char myString[1024] __attribute__((section("MY_FLASH_AREA")));You didn't mentioned how the string is programmed.
Perhaps it's during manufacture and it's immutable. If that's the case, add a const qualification to that myString declaration.