cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO WBA52CG No device found on target

Serge1
Associate II

Hello ,

I'm trying to flash in the NUCLEO WBA52CG the basic code example available in STM32CubeIDE. I use version 1.19 with Windows. It was originally version 1.17 and was updated in 1.19.

No issue to generate the code or build it. I then connected the NUCLEO WBA52CG and wanted to flash in the board.

I got the failure message "No device found on target."

 

Can anyone help me ?

I added below a pictures of the connected board. Some leds ( green and red ones) are blinking but I don't know if it's OK or not

Serge1_1-1752319133876.pngSerge1_2-1752319184153.png

Thanks in advance

Regards

Serge

 

 

1 REPLY 1
STTwo-32
ST Employee

Hello @Serge1 

does it work fine with the STM32CubeProg V2.20.0 (try different mode such as the under reset, normal…).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.