cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-L4R5ZI is not connecting to STM32CubeIde

arbio13
Associate

Hi,

I have been trying to program NUCLEO-L4R5ZI but the ST-Link doesnt seem to be connecting. I have been going through the forums and it seems the ST-Link drivers dont work with Windows 11. Is that correct?

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @arbio13 and welcome to the ST Community .

The Drivers should work without a problem on Windows11. You may try to:

  • Ensure that you are using a data USB cable and not a charging one.
  • Ensure that you are connecting the board throw the Connector CN1 and not CN14.
  • Follow the guidelines of the UM2179 specially paragraph 3.1.
  • Try using differrent USB ports on the PC.
  • Try to connect the board to Cibe Programmer, upgrade the ST-link version and do a full chip errase. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @arbio13 and welcome to the ST Community .

The Drivers should work without a problem on Windows11. You may try to:

  • Ensure that you are using a data USB cable and not a charging one.
  • Ensure that you are connecting the board throw the Connector CN1 and not CN14.
  • Follow the guidelines of the UM2179 specially paragraph 3.1.
  • Try using differrent USB ports on the PC.
  • Try to connect the board to Cibe Programmer, upgrade the ST-link version and do a full chip errase. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.