cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-H563ZI Project from Touch GFX will not show .ioc in STM32CubeIDE

PFlor.2
Senior

I created a project in TouchGFX Designer for the Nucleo-H563ZI dev kit as suggested by ST for projects that use TouchGFX.  Once created I imported the existing project into STM32CubeIDE which was fine, however the project explorer in STM32CubeIDE does not show the .ioc file even though it exists in the actual project files.

I tried to copy a link to the .ioc into the CubeIDE project explorer but when I try to open it the IDE says it's not part of the project, however I can open it in CubeMX and generate files just fine.  What am I missing?

 

PFlor2_0-1726236696291.png

PFlor2_1-1726236766007.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Principal

It is a naming issue. Rename the IOC file by replacing the underscore with hyphens. Then you should be able to drag the file onto the project and link it.

STM32H563ZI-NUCLEO-AZ2.ioc

 

Here you can see the IOC file opened after it was renamed to match the project name.

KarlYamashita_0-1726243195351.png

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

View solution in original post

5 REPLIES 5
SofLit
ST Employee

Hello,

I reproduced the behavior, I will escalate it internally. I will get back to you for any feedback. (Internal ticket number 191086)

But you can still use the independent STM32CubeMx tool to open your ioc file.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Karl Yamashita
Principal

It's probably a naming issue and some of the project files is looking for another name?

It's been awhile so i don't know what has changed in TouchGFX but here is a video that shows how to rename the project to a useful name and adding the IOC file. 

https://youtu.be/AizWAlbU4Og?si=n1cpCbG-Npb5Ivkt

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
Karl Yamashita
Principal

It is a naming issue. Rename the IOC file by replacing the underscore with hyphens. Then you should be able to drag the file onto the project and link it.

STM32H563ZI-NUCLEO-AZ2.ioc

 

Here you can see the IOC file opened after it was renamed to match the project name.

KarlYamashita_0-1726243195351.png

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

That was it...hard to see that difference with underscore vs dash.  Thanks!

I know exactly what you mean, lol.

When i added the IOC to the project, which produced the warning, my brain was telling me something isn't right. I didn't see the issue. So i deleted the IOC file and added it again. Again my brain sensed the issue right away but it took my eyes about a minute to then see the difference. 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.