2024-02-24 8:35 AM
Hi
I suddenly have a strange trap, even if i go back to a working version in Git.
Any Ideas?
Thanks and cheers
2024-02-24 8:43 AM
Hello @MFäh.1
This error message means that the debugger is trying to access the source code for the _malloc_r() function but cannot find i. I think you should check your debug configuration settings (Optimization Level, and Debug Level). For that, I advise you to check this post (not updated but it Can help) and this video. it may help you. Also, have a look at this article in the debug section: How to make sure the STM32 starts properly in our design?
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-24 9:44 AM
Thank you very much.
It helped somewhat: it no longer pops up at this location, but rather later. Is there a way to return to the previous setup (reinstall or something similar)?
Thanks
2024-02-24 9:51 AM - edited 2024-02-24 9:53 AM
Happy to know that work for you. I don't think there is steps to come back to the previous setup. You can ask for any new problem on a new post to give it more visibility so you can get more replies.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-24 9:57 AM
It worked partially as the same problem still occurs at another location in the code... so it is not really 'the solution' yet. Any other ideas? What i did was:
Project => Properties => C/C++ Build (Tree) => Settings => Tool Settings (Tab) => MCU GCC Compiler (Tree) => Optimization
In the “Optimization Level�? list box field I selected “Optimize for Debug (-Og)"
Project => Properties => C/C++ Build (Tree) => Settings => Tool Settings (Tab) => MCU GCC Compiler (Tree) => Debugging
In the “Debug Level�? list box field I selected “Maximum (-g3)�?
Cheers
2024-02-24 10:05 AM
... and do you have any insight into where this issue might have originated from suddenly?
2024-02-24 11:00 AM
Look in the breakpoints tab for any breakpoint or watchpoint you've forgotten about.
2024-02-25 7:30 AM
I reinstalled STMCubeIDE and it is working again. The breakpoints could have been an idea so.
Thank you all