2024-11-11 2:40 AM - last edited on 2024-11-11 3:08 AM by mƎALLEm
Hello. The following is machine-translated so it might seem a bit strange. I'd like to ask if I can use my only computer, the "MacBook Pro with M1 version", to connect to ST-LINK V2 to program the STM32 on a C8T6 chip's PCB board. I've tried using V1 before but without success. STM32CubeIDE couldn't recognize ST-LINK, and thus it wasn't able to program. I hope you can help me solve this problem. Thank you very much.
Solved! Go to Solution.
2024-11-11 4:41 AM
I suppose you need Mac-specific USB drivers for the ST-Link,
This applies to the standalone version and the onboard version many ST boards come with.
Those drivers are usually not installed with CubeIDE, it must be done separately.
I suggest to start with connecting the ST-Link to your Mac, and check if and how it recognizes the USB device.
I am not a Mac user, so I can't give any further hints - try a google search instead.
2024-11-11 3:10 AM - edited 2024-11-11 3:11 AM
Hello @yangyan and welcome to the community,
You need to check if your system fits the following for CubeIDE:
From the release note:
2024-11-11 3:19 AM
Thanks for your reply,I have successfully downloaded CubeIDE and compiled the program. The only problem is that I can't find an ST-LINK that is compatible with the MacBook to connect to the PCB board and perform the programming. I wonder if I can buy st-link v2 to link my Mac book P.S.I'm just a Beginner to study the operation related to single-chip microcomputers.
2024-11-11 3:21 AM
2024-11-11 3:22 AM
Does your system have macOS 13 (Ventura) or MacOS 14 (Sonoma) or not?
2024-11-11 3:27 AM
I don't know if you can accept my e-mail ,so I reply here again, it's version is Sonoma 14.6.1
2024-11-11 3:36 AM
Normally your system supports it.
2024-11-11 3:39 AM
so,I can buy stink v2?,I don't know how can I thank you with my bedly English ,thousands mile away from my you can help methane you again.
2024-11-11 4:30 AM
@yangyan wrote:
so,I can buy stink v2?,
You've already used in your first post and I don't think there is something prevent you using it.
Also there is no "C8T6" MCU part number, I think this is the final part of the part number. Example STM32F103C8T6.
2024-11-11 4:41 AM
I suppose you need Mac-specific USB drivers for the ST-Link,
This applies to the standalone version and the onboard version many ST boards come with.
Those drivers are usually not installed with CubeIDE, it must be done separately.
I suggest to start with connecting the ST-Link to your Mac, and check if and how it recognizes the USB device.
I am not a Mac user, so I can't give any further hints - try a google search instead.