cancel
Showing results for 
Search instead for 
Did you mean: 

''Log to file" info also in the Console view, how to stop that

ferro
Lead

Hi,

Can be logging done without same information being printed in the Concole view ?

When I select

[Run > Debug Configurations > Debugger > Log to file]

ferro_0-1729237957832.png

the information stored to log.txt is also sent to the Console view.

ferro_1-1729238237283.png

 

How to disable output to the Console and still have the log content ?

Thanks

Ferro

1 ACCEPTED SOLUTION

Accepted Solutions
Souhaib MAZHOUD
ST Employee

Hello @ferro 


Actually this is not possible in CubeIDE, as the log is displayed in the console output from the GDB server by default.

Thx,

Souhaib

View solution in original post

1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hello @ferro 


Actually this is not possible in CubeIDE, as the log is displayed in the console output from the GDB server by default.

Thx,

Souhaib