cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any demo Examples for STM32F413ZH discovery board?

NL.0
Associate II

Is there any demo Examples for developing UART, Audio and LCDdisplay of STM32F413 discovery board?

IDE : STMcube IDE

Discovery board : STM32F413ZHT6

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello,

Refer to the available examples with STM32CubeF4 firmware package:

STM32Cube_FW_F4_V1.24.1\Projects\STM32F413H-Discovery\Examples\UART

STM32Cube_FW_F4_V1.24.1\Projects\STM32F413H-Discovery\Applications\Display\LCD_PicturesFromSDCard

You can get inspired from existing example with STM32F411E-Discovery:

STM32Cube_FW_F4_V1.24.1\Projects\STM32F411E-Discovery\Applications\Audio

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
NL.0
Associate II

Thanks for replaying , I am having this firmware package but this project requires a conversion in order to be used with STMCube IDE.

So I am re-questioning like how to convert project STM32F413-Discovery to an STM32Cube IDE project. in order to import into the IDE

Regards, Nitish