cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX missing files: ASP256 SRAM driver for STM32N657 ?

matt-crc
Senior III

Hello,

Regarding CubeMX 6.17, I'm trying to configure a STM32N657 project from scratch.   I'm looking for the driver for the ASP256 SRAM memory chip found in various examples and the STM32N6570-DK discovery board.  If I search the "Software Packs" I can't seem to find the device listed there.  Are these files missing or am i looking in the wrong place?  I found them on Github here: https://github.com/STMicroelectronics/stm32-aps256 but I figured that it should be available in CubeMX (or it would be nice if it was available).   If they are available from CubeMX, how do I extract and add the component to the project?

 

Thanks

Matt

1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @matt-crc 

CubeMX 6.17 does not  deliver a built‑in software pack or BSP component for the APS256 SRAM (ASP256) on STM32N657, so you won’t see it in the “Software Packs” list.

The reference drivers you found on GitHub (https://github.com/STMicroelectronics/stm32-aps256) are the correct ones to use, but they have to be added manually to your CubeMX‑generated project.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.