cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a way to enlarge the icons on the ST32CubeIDE toolbar, other than fiddling with my Windows display scaling?

DHill.6
Associate

This is likely not a problem with 1080p displays. But on a 32" 4K display, even at 150% scaling, the icons are too small for my glasses prescription. Just look at those icons in my png. I've been digging into the preferences for icon size control, and I'm either looking right at it or it's not in there. And searches through your DB gives no joy. Is there some ini file I need to be editing by hand?

Dave

3 REPLIES 3
AScha.3
Chief II

you know this:

https://mcuoneclipse.com/2017/10/11/dealing-with-eclipse-and-very-small-icons-on-ultra-high-density-displays/

If you feel a post has answered your question, please click "Accept as Solution".
DHill.6
Associate

Thank you very much for the answer AND the new site to pour over. :)

AScha.3
Chief II

+ in eclipse:

>>

worked like a charm for me although I made them 150 %

-Dswt.autoScale=150

and should be repeated this goes in eclipse.ini file

also, the icons look grainy , but at least they are bigger

<<

see:

https://www.eclipse.org/forums/index.php/t/1088764/

If you feel a post has answered your question, please click "Accept as Solution".