cancel
Showing results for 
Search instead for 
Did you mean: 

Inquiry about the availability of LWIP library for STM32H563 in STM32CubeIDE

Omar
Associate

I am using STM32CubeIDE to develop applications on the STM32H563 processor, and I need to use the LWIP (Lightweight IP) library to manage network communication.

However, I cannot find the LWIP library in the list of Middlewares available in STM32CubeIDE.

I would like to know if the LWIP library is supported for the STM32H563 processor in STM32CubeIDE, and if so, how can I include it in my project?

Thank you in advance for your assistance and clarification on this matter.

Best regards.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Pavel A.
Super User

It is _not_ supported by ST (currently) and yes, you are free to download it from its home site or other STM32 package, and use.

If this seems confusing or too much hassle, outsource it.

 

Piranha
Chief II

Why are you creating a duplicate topics?

Effectively it doesn't matter whether they "support" it, because their code is a broken bloatware anyway:

https://community.st.com/t5/embedded-software-mcus/how-to-make-ethernet-and-lwip-working-on-stm32/m-p/261456

Parvez Akhtar
Associate III

Dear Piranha,

Did you hear anything from them (STM32 team) yet  for following topic ?

https://community.st.com/t5/embedded-software-mcus/http-request-to-stm32-lwip-results-that-ping-stops-working/m-p/144014

I believe they had committed to fix it by June-2023. I took multiple follow up in the same thread. No response from them yet.