cancel
Showing results for 
Search instead for 
Did you mean: 

Importing projects on second computer doesn't work

HBesi.1
Associate II

Hello,

i have problems to import projects from one computer to the other. When I import the project it looks like the first one in the picture and I cant build it or do anything with it. The second project is generated locally and works fine. Has anyone suggestions how to solve it?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Cartu38 OpenDev
Lead III

According your snapshot both are part of same workspace. Sounds not like moving from one host to another ?

By the way based on your sanpshot one folder is seen as an eclipse project the second not. So obviosuly no way to build or anything else on such second folder.

To import a project please rely on "File > Open Project From File System"

Then be aware depending of way you have created project once import will complete maybe all your project resources are not local to it ...

HBesi.1
Associate II

After importing the project it looks like this. The project is generated on another computer.